In order to cut down on LDC operation time, I wish to detect DRDY, put the LDC to Sleep then read the 4 data registers. After a delay time of 40 milliseconds or so, exit Sleep mode, and repeat.
According to the data sheet, "Sleep Mode is entered by setting the CONFIG.SLEEP_MODE_EN register field to 1. While in this mode, register contents are maintained." However, my software engineer claims that the data registers are cleared when Sleep Mode is entered. Which is correct?