Other Parts Discussed in Thread: LDC1614, LDC1612EVM
Dear Inductive Sensing Forum members.
I am presently using the LDC1614EVM (Channel 0 only) with the Teensy 3.6 micro-controller and request guidance since I’m new to working with micro-controllers.
I have two simple questions:
- I have read some where in the forum that the LDC1614EVM has a clock speed of 2MHz. What can I do to increase it internally as much as possible? Is it a simple matter of writing to the registers? The following are my settings:
writeConfig(LDC, 0x14, 0x10, 0x02); //CLOCK_DIVIDERS_CH0
- The second question is with regards to increasing the current to a maximum. The following are my settings:
writeConfig(LDC, 0x1E, 0x00, 0xF8); //DRIVE_CURRENT_CH0
writeConfig2(LDC, 0x1E, 0xF8, 0x00); //HIGH_CURRENT_DRV = b1_CH0
writeConfig(LDC, 0x1A, 0x00, 0x01); //CONFIG // Max current setting :( 0x00, 0x01 ) = 3.0 mA ?
Thank you all for your patience and guidance.
Sincerely,
Alexander Luis