Hello Everyone,
I´m a little bit confused regarding the resolution for my application. I have a inductive sensor which has a coil with L = 10,3 mH and the sensor frequency is about 25 KHz. I have read in SNOA945 that in lower sensor frequencies the Fref should also be lower to increase the resolution. In Table 4 SNOA945, for example, the Fsensor is 980 KHz and Fref is 4 MHz, that is the best resolution. I don´t know how to find the best Fref for my application. Do you have any suggestion to calculate the Fref? In the same Table 4 (SNOA945) there is a column "Output Code", what is that means? I could not find it.
Thank you very much
Best Regards