Hi I'm hyuni,
I have a confused one about table 1 of resolution at 11page in SNOSD01 and at figure 4 in SNOA944
I don't understand two data sheet to be not matching
figure 4 is that lower frequency and higher RCOUNT have an effective resolution. right?
and then
In table 1, Maximum sample rate like a higher RCOUNT has 6.5bits which is the very lower resolution
so, I'm confused cuz' not matching
please let me know that situation exactly. Thank you