Other Parts Discussed in Thread: UNIFLASH
Hi,
My customer has made some IWR1443 boards. At beginning they used ES1.0 chips. Now with same PCB, they used ES2.0 sample on board. But they failed to burn the spi flash with uniflash tool (SOP=101). Pls find the error log below. Customer already see the COM port in device manger when connecting usb with board and PC and set the right COM port in uniflash tool.
Customer also tried some other tests.
1. Using uniflash tool to burn ES1.0 customer board. There is no COM port error.
2. Try to connect customer ES2.0 board with CCS. It is connected succesfuly. This means the IWR1443 chip should boot ok. SOP=100.
3. Try to power off/power on customer ES2.0 board, and try uniflash tool. But still fail.
No matter the customer board is using 1443 ES1.0 or ES2.0, customer burn same XDS110 image on the M4 chip on board (same design as EVM). I think there should be no difference on the XDS110 image for ES1.0 and ES2.0. Pls help to confirm.
Would you pls help to advise what is missed to burn the spi flash with uniflash tool on IWR1443 ES2.0 customer board?
Thanks,