Hi.
I would like to master slave two AWR1243.
In order to do so:
1- what is the appropriate connectivity between the master and the slave of the 20GHz Clk?
2- It is mentioned that the slave FM_CW_SYNCOUT pin can be used as a loop back. How? to which pin it should be connected in the master, if at all? When you mention loopback, what did you have in mind, since the datasheet is pretty thin with information about that.
3- When using Master/Slave configuration, how should the low frequency CLK be connected?
4- What is the appropriate configuration for the Sync_in, Sync_out pins?
5- Is there a more detailed documentation about Master/Slave configuration?
Thanks!