Other Parts Discussed in Thread: AWR1443, , MMWAVE-SDK
Tool/software: Code Composer Studio
Hi,
I'm trying to start an mmWave project on CCS using mmWave link. I've included the mmwavelink.h header file and a few standard C librabries. Im following your mmWave radar programming model video and have just wrote a few lines to test mmwave link. However, whenever i try to debug my code i get an error saying:
Description Resource Path Location Type
mklib: gmake error during rtsv7R4_A_le_v3D16_eabi.lib build mklib: gmake error during rtsv7R4_A_le_v3D16_eabi.lib build mmWave C/C++ Problem
Debugging also forces my CPU to 100% CPU usage and takes a very long time. Any help would be appreciated.
Here's my starting code:
#include <C:/ti/mmwave_sdk_01_00_00_05/packages/ti/control/mmwavelink/mmwavelink.h> #include <stdint.h> #include <stdlib.h> #include <stddef.h> #include <string.h> #include <stdio.h> #include <math.h> /** * main.c */ int main(void) { rlProfileCfg_t profCfg; profCfg.profileId = 0; profCfg.startFreqConst = 0x558E38E3; }
Thanks