Hi,
My customer's IWR1443 board works ok in windows PC and now they wants to move the Linux PC.
They installed the CCS7.2 in ubuntu14.04 and the CCS works ok with the board. They saw ttyACM0 and ttyACM1 in /dev, but when they tried to connect with ttyACM0, they can't get right respond.
I tried Ubuntu 14.04 64-bit in VMware with the IWR1443 EVM and the com ports work ok. I can't reproduce the problem.
Do you have any idea/comment on the com port issue in Linux PC?