Other Parts Discussed in Thread: AWR1243
Hi, I want to develop a system in which I have a few AWR1642 interconnected composing a cascaded configuration, but I cannot see clearly which would be the hardware architecture. For what I've understood AWR1642 modules can be connected through the CAN-FD interface. On the other hand, if I want to capture all the data, do I have to use just one TSW1400 + 1 DEVPACK, or do I have to use 1 per AWR1642?