Hi Anil,
What is the SDK used in the demo given in below link.
http://www.ti.com/general/docs/video/watch.tsp?entryid=5432127759001
Regards,
Maruthi.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Anil,
What is the SDK used in the demo given in below link.
http://www.ti.com/general/docs/video/watch.tsp?entryid=5432127759001
Regards,
Maruthi.
Please find the information below:
1) This is not a real-time processing. We record the raw ADC data via LVDS interface and process the data in PC using Matlab
2) Plot 2 is after the second Doppler FFT, covering zero Doppler range profile and non-zero Doppler range profiles. The information is always available to you.
3) Again, this is offline processing. Frame rate does not apply
4) rxGain 30
adcSamplingRate 10MHz
numAdcSamples 1000
adcStartTime 6us
idleTime 30us
rampEndTime 110us
startFreq 77GHz
freqSlope 36MHz/us
txStartTime 1us
5) Ideally tracker should track any type of target. It depends on the tracking parameters configuration.
Dan
Hi Maruthi,
What Matlab code? Matlab code for signal processing or Matlab for display as shown in the video.
Dan
Hello Maruthi,
We can help you interpret data format for one our demo codes which as covered here:
mmw Demo Data Structure_8_16.pdf
Traffic Monitoring Data Structure_8_15.pdf
It would have to be up to you to use the mmWave Device data points and combine them with the video sensor of your choice.
Further more please look in to CFAR tuning parameter to change the detection thresholds.
This knob is mentioned in "tmdemo\mmwave_demo_dev\radarDemo\chains\RadarReceiverEDMA_mmwSDK\mmw_TMDemo\gui\chirpParams_TMdemo.xlsx" and passed to the device via the cfg file.
Thank you,
Vaibhav
Thank you,
Vaibhav