Hi,
I'm able to capture data from HSDCPro with Radar Studio by clicking "TSW1400 ARM" and "Trigger Frame". However, when I need to get the data next time, I need to click those two buttons again. Is there a way to continuous trigger the frame without clicking the button?
I'm able to continuous taking the data from TSW1400 using Matlab function "calllib('HSDCProAutomation_64Bit','Get_FFT_Data',TimeoutInMs, f0, df, ActiveChannelFFT, FFTArrayLength)" but I can not trigger the frame from Matlab. Any solution?
Thanks.
Best Regards
Min Liang
[unlocked 1/19/18]>LE