Other Parts Discussed in Thread: MMWAVE-DFP
Hi everyone,
according to some documents I got from TI, it is possible to configure some muxes for the 20 GHz sync signal on AWR1243. Where can I do that in mmwavelink?
We are trying to sync two AWR1243 where the 20GHz output of the master is splitted and connected to its own input and the input of the slave. It seems that the master does not require the ramp input as it also works when we disconnect it. It also seems like the slave does not get the signal as there is no usefull data captured, no matter if the 20 GHz signal is connected or not. So I guess that I have to select the source of the reference signal somewhere but I cannot find any function in mmwavelink to do that.
In an other thread () Vivek Dham said that the current firmware is not capable of supporting cascading. Is that correct or was he talking about RadarStudio? (Which is not a firmware...)
Best regards,
Fabian