Other Parts Discussed in Thread: IWR1642
Hi,
In the mmWave Demo Visualizer one of the configurable options is the maximum radial velocity. Based on chirp parameters this appears to be the theoretical max velocity. In the mmWave demo doxygen though it talks about velocity disambiguation and makes it look as though that is implemented.
Can somebody confirm if in the mmWave Demo Visualizer a max radial velocity of say 3m/s is chosen does this mean when running the demo targets up to 6 m/s will be made unambiguous?
Thanks