Other Parts Discussed in Thread: AWR1642
Dear TI,
I have two questions.
The first one is related to the high accuracy demo visualizer.
I was doing testing on short range with the AWR1642 (1 2 and 5 meters)
I wanted to test the range accuracy and resolution on different materials. Herefore i used 3 object:
- metal
- white plastic
- wooden plank
all with roughly the same dimentions of 15x50 cm.
I quickly found out when i was testing the metal object, that the radar had an offset of 8cm. This was confirmed at the web seminar last week as being due to the antenna amplifiers.
The metal object and the plastic object showed no abnormalities in further measurements but my issue was with the wooden boject.
at 1 meter i measured 1,284m
at 2 meters i measured 2,336m
at 5 meters i measured 5,324m
I did my best to find an open space with little to no object within the area to redude as much noise as possible. Is there any explanation for this?
My second question is about a situation i can't test myself.
What will happen if i put multiple radars facing each other in the same room? or a more specific setting, what will happen if 2 approaching cars use the same radar sensor?
will these interfere? is there any way to distinguish multiple radar from each other?
Thank in advance,
Alain