Hi guys,
I am trying to send data over the CAN network. I am using 2 AWR1642 devices, one sends the data over CAN other receive the data .
I connected CAN high pin to CAN high pin of the other device, CAN low pin to CAN low pin of the other device and ground to ground.
When I call the function CAN_transmitData(). I am not getting any error, but at receiver side I am not able to receive the data.
But interrupt enable field I made it 1(i.e interrupts are enabled), but call back function is not getting called.Please help me .