Other Parts Discussed in Thread: UNIFLASH, IWR1443
Tool/software: Code Composer Studio
Hi!!
I am working on mmw_mss_14xx demo code i obtained from Resource explorer in Code Composer Studio v7.4. I am using SDK 1.1.0.2. When I start the debug session, I get the following message on Console
[Cortex_R4_0] Exception occurred in ThreadType_Main.
Main handle: 0x0.
Main stack base: 0x800bad0.
Main stack size: 0x4b0.
R0 = 0x00000000 R8 = 0x0001754c
R1 = 0x00000000 R9 = 0x00014718
R2 = 0x00000000 R10 = 0x000000d1
R3 = 0x08008a74 R11 = 0xffffffff
R4 = 0x00009f8c R12 = 0x0001616d
R5 = 0x0800b2ca SP(R13) = 0x080092f0
R6 = 0x00000003 LR(R14) = 0x0001754c
R7 = 0x08008aac PC(R15) = 0x00014718
PSR = 0x400c019f
DFSR = 0x00000000 IFSR = 0x00000000
DFAR = 0x00000000 IFAR = 0x00000000
{module#40}: line 209: error {id:0x190000, args:[0x14718, 0x1754c]}
xdc.runtime.Error.raise: terminating execution
The code compiles and builds without any errors and warnings. I have loaded the code on the IWR1443BOOST board using Uniflash. Then I start the debug from the IWR1443.ccxml file.
As mentioned in other posts, i have tried debugging after resetting the board. But i recieve the same message over and over. What is wrong? Can somebody also explain what exactly is the meaning of this error.
Thanks,
Neha