Other Parts Discussed in Thread: UNIFLASH
Tool/software: Code Composer Studio
I have an AWR1642Boost board that I have previously gotten to work with the factory-loaded firmware and the mmWave demo visualizer web-app. Next step was to build firmware on my own and get it to work, so I turned to one of the Labs in the industrial toolbox, namely the 16xx flavor of the High Accuracy Range lab. I installed all the pre-requisites following the Release Notes for that lab, imported the projects to my workspace, built them.
Then I followed the instructions to load the CCS-debug firmware using Uniflash, subsequently loading the 2 compiled binary files for the DSS and MSS devices. Everything attached and loaded fine, Code Composer's console reported all was well. So I then went to the custom browser app for this demo project. It indicated that the device was connected and "Wating for data". But loading the Lab's pre-built config file did not do anything. The plots remained devoid of content. Nothing I tried changed anything. Clicking the "load config from pc and send" did not result in any messages anywhere, so I'm not sure if it's even working. Physically unplugging the AWR board left the link in the corner unchanged.
If I unplug the device and click the Serial Port from the options menu, I get a red error message saying that no serial ports were found, so at least the browser plugin seems able to communicate with the hardware. But re plugging and then clicking the "reconfigure" button does not seem to change anything. The plots stay empty.
Any thoughts what might be going wrong? I thought perhaps there was a problem with the binaries I compiled (no errors were reported, but who knows...) so I loaded the pre-compiled lab binary as per the instructions in the User Guide for this lab, but to no avail. Same behavior, no data is making it to the plots.