Other Parts Discussed in Thread: AWR1642,
Tool/software: Code Composer Studio
Hi all,
As the demo project for AW14xx in "TI resource explorer" now is based on mmwave sdk v.01.01.00.02 . For some reasons, our customized board failed with the latest image, succeed with the the previous version (project with sdk v.01.00.00.05).
I found the demo project code provided in mmwave_sdk v.01.00.00.05 (directory in packages\ti\demo\xwr14xx), but it was not a CCS project.
I've tried to create new CCS project and add these existing code into it, but failed. (I've added necessary lib and include headers)
So I wonder if I can import the demo project based on mmwave sdk v.01.00.00.05 from "TI resource explorer".
(As far I know, the projects in resource explorer are managed with version control, could any public link for us to access previous versions ?)
Or anyone tell me the steps to create new CCS project with existing demo code in mmwavesdk directory.
Thanks !
--
Lin