Tool/software: Code Composer Studio
Hello,
I want to use this board to collect data.Do you have any related learning routines?
Thanks,
Miao
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software: Code Composer Studio
Hello,
I want to use this board to collect data.Do you have any related learning routines?
Thanks,
Miao
Hi Miao,
If you are using CCS, you can extract the data you want to process:
1) Place a breakpoint in the code after the data has been collected.
2) Follow the steps in this guide to extract the data into a file: 6574.ADC Data Capture SDK1.05 V1.00 (5).pdf
Regards,
Justin
Hi Miao,
You can send the captured data across UART - this is convenient, as the usb can be configured to handle the UART data. In fact, the device is already configured like this in the mmWave Demo. However, UART is restrictive due to the low transfer speed. The device can generate much more raw data than can be transferred with UART.
If you decide to go this route, you can modify the demo found at <mmwave_sdk_01_02_00_05\packages\ti\drivers\test\mem_capture\xwr14xx> to transfer data the data it collects with the UART. You can manually collect this data by following the directions in this document:1602.ADC Data Capture SDK1.05 V1.00.pdf
Regards,
Justin