Hi ,
We are using L2 as our program memory section.
I would like to add an additional 60kbyte to L2 on the expanse of L3.
Is it possible, how can I do it.
Regards
Nitzan Tzifroni
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi ,
We are using L2 as our program memory section.
I would like to add an additional 60kbyte to L2 on the expanse of L3.
Is it possible, how can I do it.
Regards
Nitzan Tzifroni
Thanks for the quick response,
a.We need from the DSS the raw detections ,which means the objects which are detected only.
Are there some pieces of code that can be omitted from the TI code ,which are used for testing/diagnostics/logging etc.., and thus free some memory.
b. the code we have added consumes about 40K bytes in the PC and 5 times more in the DSS,maybe there is some kind of compilation directive which can be used that will reduce the code size
taking into account it's not a typical signal processing code , I know this is a long shot but I am just asking.
Regards
Nitzan Tzifroni
Nitzan,
L2 is not extendable. Only MSS TCMA and TCMB can be extended.
Reducing the size of the code, there are system print part that can be removed if have been verified. Most practical way is to remove parts that you will not need for your application.
Let me know if you have any question.
Regards,
Michelle