Other Parts Discussed in Thread: TIDEP-0091, MMWAVE-SDK
Hi all,
I was experimenting and customizing the source code of "mmWave Training - v1.6.1 /Labs/ High Accuracy Range Measurement - 14xx" to suit a level measurement application. I understand that the implementation uses two step FFT. "1 D FFT for peak search" finds the max peak and use that peak and a "Zoom in FFT for fine peak detection".
According to the docs. of this high accuracy lab, after the 1D FFT, IWR1443 is hardware is configured to search for the max peak and goes to the Zoom in FFT step.
I have a requirement of finding at least two more peaks (ordered according to the magnitude) similar to Level Sense Demo TIDEP-0091 implementation.
Which memory I should access to achieve this? Also how to access that memory? an example would be very helpful.
Can I use MMW_HWA_1D_OUT_PING memory to search for more peaks?
Cheers,
Randy