I am trying to generate standard input set from Radar Studio. I am using AWR1243Boost +TSW1400 along with Radar studio ver 1.9.2.1. I have 3 questions on this as below:
1. I tried to use the test pattern generator to generate standard data over LVDS. But the output window says "CRC FAILED". The screenshots are as below:
I would like to know why this error comes and how to rectify it.
2. In the Sensor config tab, After all the setting is done, I click on the "Set Up TSW1400" button. followed by "TSW1400 ARM", Then "Trigger Frame". No capture happens.
From the Output window, I see that When I press the ARM button, it looks for already captured data and says "No data collected". I have to repeat the ARM and trigger frame buttons multiple times beofre the HSDC pro starts capturing.
The next major problem is I am not able to stop the capture (No button press in radar studio helps) and the data doesn't get copied to the bin file. I have to power off the board and if I am lucky, some data(not all) gets copied to the bin file occasionally.
The screenshots are as below:
The output window is:
the radar studio user guide is not of much help as I see the document is not updated with the current version of UI.(I still see the Real Time button whcih was present in older UI but not in my current version)
3. In the Test Source tab, what does the signal level signify. -95dBFs is a larger signal strength or a smaller? And what range is allowable
I also would like to know how to create a test source with only one object rather than two.
Thank you in advance, for any help regarding these 3 questions.
Santhana Raj