Hi,
I am trying to work with a finer doppler resolution than the default
configuration attached to the people counting lab ("mmw_pplcount_demo_default.cfg"),
in order to still detect people at rest, in the cost of decreasing the max velocity parameter.
I am trying to work with the following configuration, but it won't work:
dfeDataOutputMode 1
channelCfg 15 3 0
adcCfg 2 1
adcbufCfg 0 0 1 0
profileCfg 0 77 370 7 20 0 0 100 1 64 5333 0 0 30
chirpCfg 0 0 0 0 0 0 0 1
chirpCfg 1 1 0 0 0 0 0 2
frameCfg 0 1 32 0 50 1 0
lowPower 0 1
guiMonitor 1 1 0 0
cfarCfg 6 4 4 0 0 16 16 4 4 50 62 0
doaCfg 600 1875 30 1
SceneryParam -6 6 0.05 4
GatingParam 4 3 2 0
StateParam 10 5 10 100 5
AllocationParam 250 0.01 5 1 2
VariationParam 0.289 0.289 1.0
trackingCfg 1 2 250 20 200 50 90
sensorStart
This config still define 6.4[m] max range.
do you know what may be the problem?
do you have a working configuration with fine doppler resolution for the people counting?
Thanks,
Boaz .