Other Parts Discussed in Thread: IWR1443, DCA1000EVM
Tool/software: Linux
Hi,
Please teach me if the following is possible.
I would like to increase the number of points displayed in the point cloud, but where should I change it?
I onece heard that Ros Driver Package can display 100 points per one object on Rviz default.
For example,can I increase this to 200 points per one object?
How many points can be displayed per one object?
--------------The details are as follows.-------------
Using:
ti_mmwave_rospkg:1.3.0
mmwave_sdk_01_02_00_05
BORD:IWR1443BOOT
I use dualboot ubuntu16.04LTS.Not Virtual Box.
I confirmed the execution and display of Rviz with the default setting.