Other Parts Discussed in Thread: ADS5294
Hello,
AWR1642+DevPack+TSW1400. I refer to the ppt "mmWave Sensor Raw Data Capture Using the TSW1400 Board".
I am using mmwave_dfp_00_09_01_06, Radar Studio v1.9.1.0 and HSDC Pro v4.90, TSW1400 can connect, but firmware cannot load into the board, shown "No firmware. Please select a device to load firmware into the board." again and again.
I can find some discussion about this question in e2e.ti.com/.../613204
In the discussion, the expert pointed out that may be due to lack of rated current of the power supply.
I checked out the power supply, "Slave, 0~30V, 5A". I set 5V, and the current knob is set to maximum.
I saw some documents, HSDC Pro v4.50 can run well, I don't know if this issue is related to the version. So can you send me HSDC Pro v4.50 download linking? I want to try again in v4.50.
Jian
Best wishes