Other Parts Discussed in Thread: AWR1642BOOST
I have an AWR1642BOOST connected to a DCA1000EVM board. I have successfully connected the the package to mmWave Studio on my PC and successfully configured the FTDI, RS232, and SPI connections. However, when I click the "RF power-up" button, I get an error that says, "Status: Failed, Error Type: RESP TIMEOUT". When I try to set up the DCA1000, I get a message that says the Ethernet cable is disconnected. I'm not sure if the two are related, but I could use some help figuring out where I am going wrong. I have tried it with the Ethernet cable connected directly to my PC and with it going through a gigabit switch, but I don't see any data in either case. Ultimately, I want to use the SensorConfig section of mmWave studio to configure my own chirps. Any advice is appreciated. Thank you!