Hi Ti
Now I want to change Modulation Frequency,I saw the chapter 7.3.5 of <<opt9221.pdf>>,My set steps as following:
1.enable TG_DIS
2.Set MOD_M1=24,MOD_N1=2,MOD_PS1=5,MOD_M_FRAC1=0;
3.Set QUAD_CNT_MAX=4
4,Set MOD_PLL_UPDATE to 1,and delay 200 ms ,then back to 0
5.Disable TG_DIS,
6.Enable PHY_TEST,enable TG_DIS
If I do step 1~6, the ILLUM_P/N is changed to 24MHZ(SYSCLK=48MHZ), but no data output, if I omit step 4, I can get test data(0~255) from OPT9221.I don't know why and want to know the step of change Modulation frequency?