Part Number: OPT8241-CDK-EVM
Hi,
We've been struggling to get the OPT8241-CDK-EVM to work properly for a couple of weeks now. After connecting it to the Rico board and running the DemoApplications we get a couple seconds of output and then "ERROR: USBIO: Bulk transfer failed.:" and "ERROR: USBBulkStreamer: Bulk End point reset failed".
Most of the time the usb disconnects with an error "device not accepting address X, error -71" and it takes unplugging and re-plugging things to get it going sometimes. Other times we have to power everything down for a while.
We tried many things to fix this, we swapped the Rico board for a i5-4200 NUC with Ubuntu 16.04; we downgraded this to 14.04, compiled pcl from source. Also we ordered the recommended power supply (newer version as the part was obsolete) and switched to an industrial USB cable. I also tried disabling the usb power management in Linux.
After that we tried a Windows 7 notebook and we see the driver disconnect and becoming an "Unknown Device". VoxelSDK sometimes works a while but with black lines trough the image, until it fails later.
As everything we tried didn't help we are thinking now it might be a bad USB connection or something like that.
Is there something else we can try to diagnose?