Hello,
Customer wants to make minimum use of LED by PDNCYCLE, but LED is not controlled with AFE4403EVM test.
Is PDNCYCLE able to make power down only internal block except LED?
So, customer wants to make LED ON only during LED가 ADC capturing by using CONTROL2 PDNTX bit ON/OFF.
At this time, Ramp Up time is not needed or need min. 50us delay as below in datasheet?
Datasheet : TI recommends setting t1 > 50 μs and t2 > 200 μs in order to ensure sufficient time for the shutdown blocks to recover from power-down
And could you recommend delay time for accurate data acquisition below each condition.
1. PDNTX bit on/off ==> ??
2. PDNTX/PDXRX on/off ==> ??
3. PDNAFE on/off ==> more than 1s (in 7.7 Timing Requirements: Supply Ramp and Power-Down)
Regards,
Nicky