Part Number: OPT8241-CDK-EVM
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: OPT8241-CDK-EVM
Dear Larry:
Thanks a lot for your kindly help!
1.
I would like to know if I can run your demo board (OPT8241-CDK-EVM) easily.
For example, I can connect the OPT8241-CDK-EVM to my Pc and I can measure the depth for my room without any programming?
2.
Do I need to buy Laser or Lens based on this board?
Does this board include laser and lens?
3.
what is the data out format of chip OPT8241?
Can I calculate the depth data based on this output by myself without the controller chip OPT9221:
( because the controller is too big )
Does TI provide this algorithm ? ( source code or Library )
4.
Does the OPT9221 also control the illumination LED/LD?
5.
And where can I download the technical document to introduce the theory of this chip?
6.
And I will write the email to ti-3dtof@list.ti.com to ask the information of the single point
Thank you!