Part Number: OPT8241-CDK-EVM
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: OPT8241-CDK-EVM
1.In door application:
The maximum ranging is between 2m~5m
>> This is achievable with TI-3DTOF
2.Error precision:
In our opinion,ToF's precision not rely on the ranging distance,and it should be in millimeter class.Right?
>> Typically 1% of max range (unambiguous range).
3.Ranging angle:
At present,we think TI's TOF ranging object is a "320x240"plane,if our understanding right,we want to know the angle of ranging.
>> If by "angle of ranging" you mean field-of-view (FOV) then the answer is FOV is determined by the lens used. You can chose different FOV lens.
In common, as for ToF method, in case the object being a point ,there will be no angle problem and the most care should be about the freshing frequency.
>> It's unclear what you mean here. Perhaps you are comparing TOF with triangulation ranging?
But in case of the object being a plane, we would need the ranging angle, and the horizontal ranging angle should be over 60 degree.
4.Refresh rate:
As mentioned in item '3', your scheme should be a plane ranging,so there is no more requirement on the refresh rate.
But if it is kind of a point ranging,the refresh rate should be over 1000 per second.
>> it is "plane ranging", frame rate if 120fps for our 320x240 product (OPT8241), and 1000 fps for our 80x60 product (OPT8320)
5.
Laser Safety:According to USA FDA on laser's certification, would it can acheive CLASS 1 for a safety laser.
Laser wavelength.
Laser optical power.
>> It is possible; in fact our OPT8241-CDK uses laser and is Class-1. All the parameters you mentioned factors into Class-1 certification.
6.Optical lens:
As the reception object is a plane,what kind of lens should be choose to use with it?
>> Usually a M10 lens with F1.1 or F1.2 f-number. Must have good relative illumination, low distortion (not fisheye); need ARC coating.
>> CRA < 30 degree, lower the better. Project image area is 1/6" diagonal for OPT8320, and 1/3" for OPT8241.