Other Parts Discussed in Thread: AFE4490, AFE4404
Hi,
I interfaced AFE4490 SPO2 EVM with K53 MCU from NXP. I can read and write registers via SPI without issues. But when I try to use ADC_RDY interrupt to read register values, value remains the same. As in RED led ADC value stays at x0003000 and IR also stays at some fixed value. But without ADC_interrupt AFE4490 gives out ppg signal.
It would be great if anyone can point out why this is happening?
Is it okay to drive LEDs at a current greater than 25mA as my application is not power constrained?