Hi, We'd like to program the OPT8241-CDK-EVM OPT9221 EEPROM without using Voxel over USB. Let's say we've made the correct wiring to the SPI interface of the EEPROM. The questions:
How should we pass the binary data from the .tie file to the SPI interface on the EEPROM? Just write every byte one by one following the EEPROM data-writing procedure? Or do we need to extract data from the .tie file, and add some other formatting header/trailer when writing into EEPROM? I red the document saying LSB first, that part is ok, but the .tie file format is unclear to me, hope someone can shed some light.
Thanks.