Hi,
I want the AFE4490SPO2EVM GUI (Ver 2.0) to come up with default setting for Capture Mode to be 'Continuous'. In the "Analysis Config.ini" file, I set the variable Mode like below.
[Active ADC Data]
# of Samples = "4096"
Channel Selection = "Channel 0"
FILTER ON/OFF = "FALSE"
Mode = "Continuous"
[INI Data Cluster IN]
Mode = "Continuous"
I do not see the change after the GUI is invoked. Could you please help me if the variable name is not "Mode" or this should be done differently.
Thanks.
=IK