I'm using the AFE4400SPO2EVM UI tool to capture LED values. Reading the register value of 0x1FFF19, how do I translate it to Volts/Codes as shown in the ADC Capture tab? I see that the register value is in Hex, and is LSB first - that leaves me with a decimal value of 1703711 while the ADC capture page shows a range of ~100,000 in Code and 0.05 in volts.