Hi all,
I'm planning to interface a single-board computer with 8 AFE4403's over SPI. The SPI bus will be in a star configuration with each of the slaves separated from the master by up to 15cm of cable.
1. Is it possible to daisy chain the SPI data lines so I can free up some GPIOs that would be used for a 3-to-8 slave select decoder? The AFE44xx datasheets do not specify such a capability, but I figured it might be worth asking anyway.
2. Due to the distances and number of devices loading the bus, is it recommended to use some sort of buffering and/or terminations on the SPI bus? What components and/or design schemes do you recommend?
3. In the event that I cannot source a low-jitter (<50ps) clock output from a single-board computer and have to resort to having crystal oscillators on each AFE, how will this affect communication between the AFEs and the processor? I am considering clocking the SPI bus at 1MHz. I am also planning to average the ADC samples as much as possible with the AFE.
Thanks,
Robert