Other Parts Discussed in Thread: AFE4490
Tile: AFE4490SPO2EVM USB connection and powering problem. Thanks!
Hi TI experts,
I am trying to connect AFE4490SPO2EVM with Arm TivaC LaunchPad, via USB port. The questions are as follows:
1) Can I connect the EVM with Launchpad, as USB slave and master, respectively ?
2) How to power EVM, since its USB is connected with Launchpad, no PC? How to connect external battery, and configure the board for power source selection?
3) How to power the Launchpad? Since there are two USB ports on Launchpad, can I use one to connect with EVM, and another to get the power? Or I need use external battery and how?
Thank you very much. Waiting for reply since we need to determine the solution and purchase the product now.
Best
Jackie