This is an initial general query to check the suitability of TI products for the appliaction.
It is an offshore application where a crane must lower equipment very accurately into the sea.
We in Horizon Survey used to perform such installation using survey sensors DGPS, GYRO and IMU interfaced to online navigation system Qinsy.
The new scope is to monitor the structure during installation for accurate position, heading and tilt. The structure would be carried by a crane from the lifting barge or heavy lift.
For above purpose, the laser tracker, Lidar or 2D / 3D camera/s shall be used in addition to the assist from survey sensors (DGPS, GYRO and IMU). Qinsy generally used to interface survey sensors.
You may add any kind of targets and you could be provided with the structure in 3D prior to the operation.
Attached image may provide with better understanding, but please let me know if you still missing some clarification.
Please see this video : https://youtu.be/yPjmhnx0g3w
I’m really looking for your quick response as quickly as possible.
I will pass this to commercial team with your positive response as they are bidding for something similar at the moment.
The Project main target would be “Client Requirement”:
JACKET POSITIONING
The location and orientation of the jacket shall be as specified on the contract drawings. SUB-CONTRACTOR shall check the jacket set on the seabed to the following tolerances:
Jacket position range: +/-0.5m of the specified jacket coordinates
• Verticality : +/-0.2°
• Heading : +/- 2.5°
EQUIPMENT REQUIREMENTS
To carry out the services required, SUB-CONTRACTOR shall provide the minimum equipment, hardware, data QC software and personnel as specified in this documents.
The positioning sensors shall be installed on board of CONTRACTOR vessel and use a vision based technology that track the position of Jacket and give a real-time position, elevation and inclination and heading of the Jacket, the positioning sensor shall be interfaced with CONTRACTOR Navigation Software and have the following accuracy:
• +/- 0.xm relative position and elevation ;
• +/- 0.x° relative heading;
• +/- 0.x° pitch and roll;
The key advantageous points that should be on our solution should be:
- Minimal equipment on the structure to be installed; however if you may need targets for the OPS. We can add.
- Minimal personnel interface with structure to be installed.
- IMU integration for the Barge / Lift vessel motion compensation.
- Final would be the ability to interface the same with our navigation systems or to get absolute values from it to be shown on our NAV system.
I kept the relative tolerance in grey and you may fill it with figures that you think achievable with confidence.
I saw many products on you website that may help in this application, so could you please get in touch; hence we can work together on this project.