Part Number: OPT8241-CDK-EVM
Hello.
I'm working on my final bachelor project. I managed to get extrinsinc and intrinsic parameters of the hybrid camera system using Matlab Stereo Calibration app. The next step is really vague. How can i align depth with color infrmation to make a colored point cloud? Most of the sources are using Kinect V2 to make these point clouds and Matlab even has some special functions to get it working. I couldn't find any topic realted to OPT8241 CDK and RGB camera mapping. Right now I'm using RasoberryPI to acquire RGB image in the same resolution as the ToF has - 320x240. Later on I'm planning to use a camera which has a greater resolution and connects to PC via USB. Wanted to find out if anyone has even tried it? Is it even accomplishable? And if it is what are the next steps I should take to get the system working?
Any information will be much appreciated!
Regards,
Andris