Part Number: OPT8241-CDK-EVM
Hello,
Thank you for replying my previous questions.
We are planning to make our own illuminators and driver board, then connect with the current OPT8241 sensor board. The purpose is to use more powerful LD/LED to see the further distance objects.
Here are some questions:
1) The trigger(integration) and modulation signals are controlled by the TFC, our driver board should have two main functions: 1. response these signals; 2. output the proper power amplitude during the integration period. TFC will be responsible for triggering the driver board and control the modulation frequency, correct? Are there adjustable through program?
2) If 1) is true, which means the driver board only drives the LD/LED when it receives the trigger(integration) signal, it then control the output power to the certain level, since the frequency is controlled by the TFC.
So the output power from the driver board is equal to the peak power of the 3D ToF System Estimator Tool, correct?
3) Are there any technical issues we should be aware of our application?
Thanks,
Yun