Hi, could someone verify the value for the current responsivity of the diode.
According to the datasheet on page six, where the specs for the optical sensor are listed, there sits a value of 865 (uA/W)/cm2.
Either I don't get its meaning or I'm stupid (most probably both !)
If I get a responsivity R = 0.45 A/W for uniformly illuminated phd with a sensitive area Sphd = 5.2mm2 when I divide R/Sphd I dont't get the number listed. Why?