Hi TI:
I encountered the following problems in the calibration process
- When the offset calibration, such as the need to super - HDR mode of four groups of current value, whether to phase four groups of calibration current, and the four offset value written to the corresponding register, so whether we need four groups in the offset correction current measurement process meet the AMP > 10000?
- In offset correction under the condition of four groups of current (choose only one group for correction of current measurement of AMP > 10000), in this case, when running in super - HDR mode and under a certain distance measurement, when the current group will lead to larger distance migration, there is no accurate calibration result in?So does the switching of current cause a large deviation in distance?
Look forward to your reply!
Best,
Kevin_Wang