I am trying to using the PGA900 to output data on the UART as quickly as possible. it seems that the UART should be able to go up to 250kbaud (baud divider at 0). However when I set the baud divider at 0 or 1 the UART doesn't seem to work anymore. At 2 it generates the expected baud of 83.3 kbaud but it seems to shutdown below that. Is 83.3 kbaud the maximum?