Hello,
I am trying to design an anti-aliasing filter for the PGA900. I know the sigma delta modulator frequency is 1MHz, but I am not sure if this means the Nyqyuist frequency is 500kHz. The other possibility is that since the max output rate is 15.625kHz so I also thought the Nyquist frequency might be 1/2 this or 7.812kHz.
Below is my filter as currently designed. I was thinking about reducing the capacitors by a factor of 10 to 0.1uF and 0.01uF. Before doing this I wanted to make sure that the Nyquist rate is 500kHz and not 7.812kHz.
Thanks,
-Hunter