I compile sample code and pga900.hex is generated. Currently I am facing 2 problems.
Problem #1:
PGA 900 EVM is configured in voltage mode. Supply voltage is 12V. Sample code is loaded to core. Now PADC_DATA is changing according to input analog voltage. But DAC_REG0 is not updating according to sample code.
Problem #2: Without PGA900 IC in EVM board voltage at J12 (OWI) pin is 5V. But with PGA 900 IC voltage at J12 (OWI ) is becoming 7.5 V. Can anybody tell the reason for the same?