Other Parts Discussed in Thread: USB2ANY, PGA970,
I have PGA970EVM and the USB2ANY connector that came with it. I have installed the PGA970 GUI and other software and core files (sldc015 and sldc016) The installation progressed smoothly without any errors or warnings. I have installed the required LabVIEW when I was directed to the NI website from the installation.
I have a dell laptop with USB3.0 ports and Windows 10 Pro Version 1607 Build 14393.576.
When I connect the USB2ANY to my laptop, the green LED lights up but when I start the PGA970 GUI it cannot find the hardware and runs only in 'Hardware Disconnected' mode. Are there other settings that I need to follow? I checked it under the system management and nothing showed up. So I am guessing that some drivers might still be missing, but any help is appreciated.