Hello,
After a considerable time spent in the documentation and looking through the source code for the example firmware - I have been unable to answer the following question:
What is the lowest power mode available and what is the average IDD/uA consumed in those mode?
So far, I've only been able to find is the IDD Max (which is 2.8ma).
I see in PGA900.pdf datasheet "Refer to ARM_M0_User_guide.pdf for M0-specific register addresses" - so I'll assume these registers are available?
Can I use the standard WFI/WFE M0 registers then? Assuming I can, has anyone measured the IDD comsumption in these low power modes?
I need an answer to this question before I dive in and buy a PGA900EV.
Thanks!