This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PGA970: Need help configuring the PGA970

Part Number: PGA970

Hi 

i have got a PGA970, and trying to interface with an LVDT.

I and able to communicate the PGA970 to GUI with the help of USB2ANY, and tried configuring the same.

I tried configuring the PGA970 for the LVDT primary frequency of 2.5Khz with the amplitude of 2.5V.

In the GUI the max Amplitude possible is only 0.375V.

can anyone guide me on how to set the amplitude? is there any formula available to calculate the same?

Also i need to read the LVDT position on SPI, is this possible? if yes kindly let me know the register which i need to read for the position.

Looking forward for your support.

Shivu

1 Reply

  • Hi

    In PAG970 GUI User’s Manual,  there is "In Single-Ended Mode, WFM_Amplitude < (WFM_Bias - 0.15)/GAIN_CTRL, In Differential mode, WFM_Amplitude < 1.235 - WFM Bias".

    If  you want the amplitude of 2.5V, you should use the EVM' hardware amplifying circuit.

    And  I also wonder where is the LVDT position? In GUI I only to find ADC1 and ADC2 data.

    Thanks!

    Wang Jie

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.