My customer is trying to get the TMP007 EVM alert mode to clear. Can this mode be tested on the EVM? See below:
I would like to test the TMP007 in comp mode. My goal is to have the software set up the sensor…and have the alert pin control the heater. The demo GUI I have does not seem to allow “COMP mode” as described below. Is this possible with the demo? Could someone provide the “magic settings” that enable this mode of operation?
7.4.2 Alert Modes: Interupt (INT) and Comparator (COMP)
The INT mode maintains the alert condition until a host controller clears the alert condition by reading the status
register. This mode is useful when an external microcontroller is actively monitoring TMP007 as part of a thermal
management system. The COMP mode asserts the ALERT pin and flags whenever the alert condition occurs,
and deasserts the ALERT pin and flags without external intervention when the alert condition is no longer present
This mode is often used to notify an external agent of an alert condition.
When servicing an alert from the TMP007, in some cases it may be useful to validate the alert condition by
checking the status of the nDV, MEM_CRPT, and DATA_OVF flags.
20
Regards,
Aaron