Figure 24 shows the small-footprint layout modified by adding 10mil per side for shield mounting.
The 3.25mm dimension shown is inconsistent with the small-footprint layout in Figure 17. That shows the copper area being 130mil wide, which is already 3.3mm.
Which is correct? Should the copper area width be increased to 3.3mm + (2 x .25mm)?
Does the 200mil dimension in Figure 17 expand by .5mm to maintain the copper-free gap size?
Whichever is correct, to the same adjustments apply directly to the large-footprint layout, or would it be a proportional adjustment? What about shield adjustments for the Laser Cut Micro Footprint?
The guide doesn't spell out whether the small copper fill in the center of the footprint should have soldermask over it.